Recent Posts

Pages: 1 ... 6 7 [8] 9 10
71
Displays / Re: Changing image size in program? vector editor
« Last post by Marbek_Elektronik on March 13, 2024, 10:00:47 PM »
Thanks,
but I don't understand your second image.

I don't find "signal input"
(it is svg format)
72
Displays / Re: Changing image size in program? vector editor
« Last post by Lukey on March 13, 2024, 02:44:23 PM »
I believe it is, I have not done/tested this exactly but I imagine you could create a text/image widget.
Set ScalePos and ScaleSize to True for the object in the Widget.
For the Widget property set the Width and Height externally with an input.

Some combination of the above should achieve the outcome.
73
Displays / Changing image size in program? vector editor
« Last post by Marbek_Elektronik on March 13, 2024, 12:57:46 PM »
Hi,
is it possible to change image size by running?

I want to change font size and image size by run-time.

Currently, I only know that this works before compiling and then the size is defined.

(Rotation ist possible, i know)
74
PLUS+1 GUIDE / Re: Missing fonts error when trying to compile with 2024.1
« Last post by williamk on March 06, 2024, 06:08:52 PM »
This appears to be fixed in 2024.1.4
75
Controllers / Re: Parameters not visible
« Last post by SVK on March 06, 2024, 01:42:51 PM »

I found what was wrong.
The OS was different, all parameters became visible when I updated the OS.

Thx for the help though.
76
Controllers / Re: Parameters not visible
« Last post by Tor on March 06, 2024, 08:25:09 AM »
Hello SVK,

If you open the service application in an earlier version of Service Tool does it work?
In that case I would recommend you to create a case for PLUS+1 Helpdesk:  https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-support

If there have been a name change for some reason, you need to open the service screens and change the signals to the correct ones. I have marked in the attached image where to look when using a regular parameter component in Service Tool.
If you don't have permission/access to do this, I would recommend you to contact the developer of the service screens or the machine manufacturer.

Have a nice day,
77
Controllers / Parameters not visible
« Last post by SVK on March 05, 2024, 01:45:35 PM »
Hi all,

I have a project file that dates from 2016. When I open it in the latest Plus+1 service tool some parameters are not shown because they don't exist or have another name.
How can I fix this issue?

The parameters I haven't found yet are:
EE_DOutSpd_rpm1
EE_DOutTorque_Nm3
EE_MagCurrBoost_pct2
EE_SnsrSupplyVltg
EE_SpeedCalcMode
EE_SpeedFOF_ms
EE_VCellRst_mV
SpdInvSgn
Val1 To Val10
78
Displays / Re: Lifetime NVmem Erase/Write for DM430E
« Last post by Tor on March 05, 2024, 01:41:32 PM »
Hello,

Sorry about the late response.

I was approached by a developer who saw this topic and he wanted me to write a clarification to avoid confusion.
When it comes to the DM430 and the EEPROM we guarantee 4 million write cycles.


Have a nice day.
79
Displays / Applog size and memory usage
« Last post by Lukey on February 29, 2024, 06:35:03 AM »
Hello, i am using a DM1200T.

Is there anyway to ready the 32mb applog memory size to determine how much has/is being used?

Reading the OS.RAM and OS.Flash values indicates that the applog memory usage has no influence on these values, as I cannot see an significant changes when writting/reading to the applog memory.

The Write_USB block (designed for the DP720 does not work with this hardware fully) does not give information on Used_Blocks or Free_Blocks unfortunately.
80
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by Egholm-Jonas on February 28, 2024, 01:32:21 PM »
With some help from Tor, I can move on again!! :)

The invalid character '0xBB" error was caused by the checkmark in "Regions Settings" on my pc. (See attached picture)

Why this was selected I have no idea! But this did it for me! :)
Pages: 1 ... 6 7 [8] 9 10