PLUS+1 Software > Sub System Applications
Compiling with SSA Blocks in program
(1/1)
Nick Anderson:
I am trying to compile using the Fan Drive SSA block, and I continue to get an error saying *** ERROR 309 *** [CHPARGU1] APPLICATION BLOCK IS LOCKED TO HARDWARE {10106603}. Reading through some things, it looks like you have to have keyed hardware in order to load a program containing an SSA onto the controller, but there shouldn't be a restriction on compiling it to create your downloadable file, right? All help is appreciated.
Slashe:
Hi Nick!
You should try this. There is a place for Target part number in the project manager tab in the GUIDE. You should try to enter the number (10106603) there and then try to compile.
Slashe
Navigation
[0] Message Index
Go to full version