Author Topic: Problem with Widget library  (Read 8221 times)

Offline samuelhj

  • PLUS+1 Developer
  • ***
  • Posts: 22
  • Karma: +0/-0
Problem with Widget library
« on: December 15, 2024, 06:04:17 PM »
Hello.

Been a while since I had to program a display, but I'm running into two seperate issues.
Display type: DM430E 0-1-X-X series.
Guide version 2024.4.3

If I add a gauge, adjust parameters, and try to compile I get compiler error.
See attached screenshots.

Another strange issue I noticed, linear gauges do not even fit the display, but since I've never used them, I'm not sure if this is expected behaviour?