Author Topic: DP250 Power Consumption  (Read 5466 times)

P!nk

  • Guest
DP250 Power Consumption
« on: May 21, 2013, 02:42:56 PM »
I am planning to use a Sauer Danfoss in a battery powered application (using Ni-Mh) and I am thinking of using the DP250. The problem I have is the power consumption, from the datasheet it is 6.5W or about 677mA at 9.6V, this will flatten a 2AH battery pack in under 3 hours.

I was wondering if anyone on here has any experience of using these displays in a battery powered application and what advice they could give to extend the battery life, ideally the batteries need to last for 8 hours.


Any advice you could give would be appreciated.     

Offline niteRider

  • PLUS+1 Developer
  • ***
  • Posts: 45
  • Karma: +3/-0
Re: DP250 Power Consumption
« Reply #1 on: May 21, 2013, 10:17:03 PM »
I'd start with turning off the heater and reducing the backlight as much as possible (look in Outputs-->Display).  If you have the display driving any lights, then consider using a relay or LED to reduce consumption.

Other than that... probably not much you can do.

good luck...

P!nk

  • Guest
Re: DP250 Power Consumption
« Reply #2 on: May 25, 2013, 10:29:47 AM »
Thanks for your help, I will give it a go.