PLUS+1 Hardware > Controllers
Changing Input config on the fly
Undertow:
Hi,
Anyone know if it is possible to change the pin config on a controller pin on the fly e.g. via display or service tool?
I want to use the input as resistive for now but the customer in the future wants to use 0-5v I/P, can this be done?
Thanks
Gregor:
I have changed the pinconfig of output pins via "switch" for a small hydraulicvalve testbench, we use at our workshops.
Greetings Gregor
Undertow:
Thanks Gregor,
I have made the change and it seems to compile ok but don't know if it works (but I think it should).
Thanks again
Larry
niteRider:
You may have to power cycle the controller/display for the pin config to take effect...
Richard:
I just added a switch (bool controlled) to change the pin config on an MC5010 and it would not compile until I deleted the INIT symbol connected to the config wire. Maybe it's template dependant but I got a compile error message along the lines of ' invalid output connected to component'. Switch outputs are not compatible with INIT symbols.
Richard
Navigation
[0] Message Index
[#] Next page
Go to full version