PLUS+1 User Forum

PLUS+ Tools => PLUS+1 GUIDE => Topic started by: ET on April 16, 2012, 03:45:16 PM

Title: Pulse which holds sinal for duration even if input signal goes T/F.
Post by: ET on April 16, 2012, 03:45:16 PM
The help docs state that the Pulse component will output false if the input goes T/F during the hold time.
Is there another component which will continue to output true for the entire hold time, even if the input goes T/F during the hold time?
If not, is there an easy way to wire this function up using other components?
Title: Re: Pulse which holds sinal for duration even if input signal goes T/F.
Post by: A.Peterson on April 16, 2012, 07:25:48 PM
Use a positive transition into a delay off and you can set the length of pulse to whatever you want regardlees of the input state.
Title: Re: Pulse which holds sinal for duration even if input signal goes T/F.
Post by: ET on April 17, 2012, 07:09:17 PM
Ah, that sounds like it will work nicely.
Thanks!