PLUS+1 Hardware > Controllers
Joystick with Duty output
(1/1)
sverreo:
I have a joystick that output a 5V 500Hz Duty signal.
Can anybody explain how the duty input on f.ex. C1p16 on an XL104 work and should be setup?
I looked throug the API, but it doesn't give a thorough explanation.
The settings that work best for me is:
Bias = 3: Pull-Down to internal GND, Pull-Up to internal +5V
Range = 0: 5,25V range
Are the DigThresHigh and low settings applicable when using duty?
I say those settings work best for me, but i have had insidents when suddenly the input can't read the duty signal and only oscillates between 0 and 100% in the servicetool when i know the duty is 50%
sverreo:
Heres my settings atm
Navigation
[0] Message Index
Go to full version