Author Topic: Read Array from Application Log  (Read 8215 times)

Offline hgb1992

  • PLUS+1 Developer
  • ***
  • Posts: 13
  • Karma: +0/-0
Read Array from Application Log
« on: June 10, 2013, 10:09:20 AM »
Hello!

I want to use some DP2xx Display for application logging. But I need the logged data in application too.
I have to write the value into the app log and in the next program loop I use this data for calculation the new value for the app log (like a RAM).

Can I use the function "Read Arry from Application Log" with any DP2xx? Because in every .hwd I tried, the function was disabled.

Will this use generate some problems with the storage or anything like that?

Thanking you in anticipation!

Kind regards,
Benedikt

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Read Array from Application Log
« Reply #1 on: June 11, 2013, 10:28:41 AM »
Hi hgb1992

The "Read Array from Application Log" is for the moment only available for DP6xxLX display hardwares.
Have you considered using the NV-memory?

Best regards
Daniel
Plus+1 HelpDesk
PLUS+1® Help Desk Team

Offline hgb1992

  • PLUS+1 Developer
  • ***
  • Posts: 13
  • Karma: +0/-0
Re: Read Array from Application Log
« Reply #2 on: June 12, 2013, 10:18:14 AM »
Hello Daniel,

thanks for your answer.

I didn't think on NV memory, because it has a limited opportunity for overwriting. Do you know the detailed quality of possible overwrites?

I will write on the memory several times per second, therefore I think the NV will have a defect after short time.

Do you have a good suggestion for a cheap solution without a DP600LX, because the user only needs a very easy display and a "save" value also after supply disconnections. So I have to save as much.

Thanking you in anticipation.

Kind regards, Benedikt

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Read Array from Application Log
« Reply #3 on: June 12, 2013, 12:57:23 PM »
Hi

When it comes to displays, the NV memory can be used without limit since they are using FRAM as a memory instead of EEPROM (that is otherwise commonly used among controllers).

So the NV memory should be possible for you to use in this case.

Best Regards
Daniel
PLUS+1 HelpDesk
PLUS+1® Help Desk Team

Offline hgb1992

  • PLUS+1 Developer
  • ***
  • Posts: 13
  • Karma: +0/-0
Re: Read Array from Application Log
« Reply #4 on: June 13, 2013, 10:24:03 AM »
Hello,

thanks for your help.
So I will try with DP200.

Kind regards,
Benedikt