PLUS+1 Hardware > PLUS+1 Compliant Hardware

Joystick ProGrip

(1/1)

Quax76:
Hello everybody,

does anyone has any experience with CanOpen Joysticks from SauerDanfoss?
I want to use a ProGrip but don't know how to configurethe good boy...

Jakob:
It pretty easy if you use the function blocks provided by Sauer-Danfoss.
Just connect CAN-bus channel to the CAN pin, and set a value on the SA pin.

SA 0x33 hex is the right joystick
and 0x34 hex is the left.

I hope this helps.

Quax76:
Thanks...
But this only works, if you use a baudrate with the default Value (250k).
My intention is to change the settings of the joystick, but SD only provides an EDS file and my PCan Explorer doesn't support eds.

Navigation

[0] Message Index

Go to full version