PLUS+1 Tools > PLUS+1 GUIDE
CHPARGU1 - INTERNAL UNEXPECTED EXCEPTION
(1/1)
ShadowRam:
I got this error today while trying to compile a program.
(This is an existing program that has worked fine, that I just did a few simple changes too)
ERROR 302 CHPARGU1 INTERNAL: UNEXPECTED EXCEPTION WITH MESSAGE: {Access violation at address 004CCEC0 in module 'chpargu1.exe' Read of address 00000007}
What is this? It doesn't really give me an idea of where to start looking for the problem.
Thanks,
Stefan:
Hello,
Please send this text and your P1P to helpdesk@sauer-danfoss-plus1.com so we can have a look at it.
Best regards
Stefan
ShadowRam:
I isolated the problem and found what I did. ;D
I have two PGN 61445 modules each with different 'Source' Address and the 'Use Source' set to True for both of them.
This worked and I had no problems.
Recently I changed one of 'Use Source' to False, and it caused this error.
Makes sense why it doesn't work, but it was a pain to track down, hopefully you guys can add something to the compiler error messages that would help the next guy that makes a similar mistake.
Thanks,
Navigation
[0] Message Index
Go to full version