Author Topic: measure the weight load on cranes  (Read 12257 times)

DENIS

  • Guest
measure the weight load on cranes
« on: January 17, 2011, 01:27:16 PM »
Good morning ladies,
need to make the measurement of weight of the load hoisted from a crane, using a pressure transmitter installed on the lifting cylinder of the boom, according to the radius of action varies with the pressure transmitter, anyone have a clue how to do this logic?

bgtwuk

  • Guest
Re: measure the weight load on cranes
« Reply #1 on: January 18, 2011, 04:19:56 AM »
How will you monitor the radii?

Bgtwuk

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: measure the weight load on cranes
« Reply #2 on: January 18, 2011, 08:41:13 PM »
Hi there.

I'm currently looking at a similar application. You may wish to review the mechanical principles of a” third order lever" typically which most crane applications fall under. I have a draw wire displacement sensor to monitor the boom extension and retraction. This will be useful in adjusted the load position as the boom extends or retracts (load positioning)
F= cylinder force
a= boom extension

Force on the cylinder is f= pressure x area.





Jelmer

  • Guest
Re: measure the weight load on cranes
« Reply #3 on: January 31, 2011, 09:32:00 PM »
In theory this is correct, however in real-word you also need to calculate in the angle in which the force is applied. (the force in relation to the beam and the force of the cilinder in relation to the beam). Futhermore this angle changes during operation.

To make things more dificult....you also have to calculate the slip-stick of the cilinder. Normaly the load is messured by using a loadcel underneath the upper pully of the beam.

All depands on how accurate your system has to be.

Good luck

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: measure the weight load on cranes
« Reply #4 on: January 04, 2016, 11:13:55 AM »
It's very late.
But perhaps this helps:
http://www.intermercato.com/
They can measure the load by moving the crane.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Kava_Man

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
    • LIVE Magazine
Re: measure the weight load on cranes
« Reply #5 on: March 11, 2019, 11:15:36 AM »
It's very late.
But perhaps this helps:
Performance Lab SPORT Fat Burner
They can measure the load by moving the crane.

It is late but it's always worth posting if you're linking to a reliable source. People might not be talking about a topic anymore but there are people like me who visit these forums to look through old answers before bothering to post the same question again. Thanks for linking this anyway man, very helpful!
« Last Edit: March 13, 2019, 10:26:20 AM by Kava_Man »