Author Topic: Making a Sound when ready with compiling  (Read 5529 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Making a Sound when ready with compiling
« on: May 25, 2013, 12:01:53 PM »
Hi,

if I have a big program, I do anything else by waiting.
It would be nice, if the computer gives a sound when guide is finished!
So, I can come back to my computer and go on with downloading the file to a controller.
After downloading is ready, it would even be nice, if the computer produces a sound.

What do you think about this nice feature?

Bye,
Bernd
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: Making a Sound when ready with compiling
« Reply #1 on: May 25, 2013, 10:29:07 PM »
Hi Bernd

I would like to have these features.

They would be nice to have as you say when working with a big program.
But a simpel checkbox to disable the sound, will probably be equally nice to have if you are testing something in a small program.

Good idea, Bernd.

regards Jakob

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Making a Sound when ready with compiling
« Reply #2 on: May 28, 2013, 08:54:46 AM »
Thank you.

We have added it to our wish list for future improvements.

Best regards
Daniel
PLUS+1® Help Desk Team

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Making a Sound when ready with compiling
« Reply #3 on: May 28, 2013, 11:32:25 AM »
Thanks!
 :)
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Making a Sound when ready with compiling
« Reply #4 on: April 10, 2014, 10:16:35 AM »
Hi Daniel,
when will it be implemented in new Guide software?                                   
It is not so important, but nice to have  :)
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Making a Sound when ready with compiling
« Reply #5 on: April 29, 2015, 07:13:02 PM »
Hi Daniel,

now, it is 2 years ago.
Whats about the sound, when compiling is ready?

Another question:
Is it a problem to use Strg+F5 ?
Somebody tolds me, not to do this. Perhaps he had had trouble in an old guide version?

Should we use the partial compiling function = Strg+F5 ?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Making a Sound when ready with compiling
« Reply #6 on: April 21, 2016, 09:55:47 AM »
Now, 3 years and no sound  :(

Compiling needs 4 minutes and it would be nice, if computer gives a sound, so I can do another thing and don't need to watch to monitor.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: Making a Sound when ready with compiling
« Reply #7 on: April 25, 2016, 12:45:56 PM »
Hi Bernd!

We still have this in what we call our wish-list but unfortunately it hasn't been implemented yet.

Today the standard shortcut button for Compile all is F5 and Compile changed is Ctrl+F5. If you want to you could change the buttons under Setup -> Options -> Shortcuts -> Application. We haven't heard of any problems using these shortcuts.

Best regards,

Nilla Troedsson
 PLUS+1® Helpdesk