Author Topic: hwd files  (Read 4726 times)

paterianus

  • Guest
hwd files
« on: July 19, 2011, 10:28:42 PM »
If I download a new hwd file from the S-D web site are the new feaures automatically included the next time I compile a project or am I required to manually delete and re-install the associated hardware?

Offline Richard

  • PLUS+1 Expert
  • ****
  • Posts: 64
  • Karma: +2/-0
    • Textron
Re: hwd files
« Reply #1 on: July 20, 2011, 11:03:31 AM »
You need to change the HWD file in the application manually.

First you need to install it in GUIDE.  Go to setup/install hardware then you see it appear in the Hardware tab on the right.  Then either drag the sys file from the right to the project manager tab/sys file on the left or right click on the new hardware file and select 'use this hardware in project'.

Hope this helps.

Richard


Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: hwd files
« Reply #2 on: December 04, 2013, 08:34:53 AM »
Do you prefer to use the newest HWD-File (sys-file) by opening a project in a new Guide version?

I want to open older projects from Guide 5 and I want to do some changes.
One way is to import the project an do the changes.
The other possibility is to change the sys-file at first. Could this produce new errors?
Is it better to change the sys-file?

Bye
Bernd Konrad
Marbek Elektronik
(Germany)
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung