Author Topic: J1939 NON INCENDIVE- DANFOSS CAN BUS INCENDIVE OR NON INCENDIVE?  (Read 5223 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
this may be for Nilla,

I know Danfoss products are designed for off road machinery.  so mining uses also off road mchinery...then a problem pops up, it needs to be in compliance for the dangerous area, in other words, intrinsically safe or explosión proof.

Now, one thing that engine manufacturers do is that their ECU comes already approved for it. basically they separate the Incendive signals from NON INCENDIVE signals.

J1939 communications protocol becomes a NON INCENDIVE signal so I cannot interface directly DANFOSS CAN with  J1939 non incendive becuase nothing tells me that the DANFOSS CAN is also a non incendive signal ...and of course the issue starts at the DANFOSS connector all signals are together.

my question is:

Could the DANFOSS CAN bus be a NON Incendive Signal?

if not, Has Danfoss Ever considered this option?

I appreciate any feedback about

Thanks