Recent Posts

Pages: 1 ... 8 9 [10]
91
Controllers / Re: IX024 and SC024 using Primary and Ssecondary
« Last post by Matt_Eng on June 18, 2021, 02:42:52 PM »
Hi, the easiest way is to include the IX024-10 block in the primary and secondary. Then setting enable to false in the secondary application.

Only thing that may be useful to be handed over from primary to secondary are the Configured and CommStatus signals on the CAN sub-bus. E.g. Inputs->CAN->Configured
To hand the data over from primary to secondary, you will need to use the UART channel. The safety library has some function blocks that can help with that.

Best regards, Matt
92
Displays / Re: DP710 - no images but everything else seems to work [RESOLVED]
« Last post by PatrickS on June 18, 2021, 02:05:42 PM »
I found out that the LCD in the display has had some hardware changes and requires the hardware file for the DP710 to be updated to the latest version.
93
Displays / DP710 - no images but everything else seems to work [RESOLVED]
« Last post by PatrickS on June 17, 2021, 03:23:48 PM »
Hello,
So we've been programming DP710 with this same code for years without issue. Then yesterday we went to program a display, it started up alright showing the Danfoss logo, however; after we were done programming it, no images show on the screen.
We thought maybe the display unit was damaged so tried another one, same issue.

You can tell the backlight is on and we still have communication with the buttons. We can also see that the logic of our program seems to work as we can go through our menu on service tool but nothing shows on the display.

Also, not sure if relevant, but we noticed that the screen was getting abnormally hot during testing, at least to 100F.

Any help is much appreciated,
Thank You
94
Controllers / IX024 and SC024 using Primary and Ssecondary
« Last post by macbahi on June 17, 2021, 02:24:45 PM »
Hi!

Please I want to use some input from IX024-010 in primary and secondary S024-120.  My question is I must to use
double expansion IO_Module in primary and in secondary or exist other way to have access to input IX024-010 in secondary SC024-120.

Thank you very much

Best regards
macbahi
95
Telematics / Re: Notifications
« Last post by Tor on June 17, 2021, 09:28:10 AM »
Hello,

Since I don't have much knowledge about the PLUS+1 Connect Portal, I would recommend you to use the support function in the Portal (see image) if you don't get any answers here in the near future.
I asked around and there should be possibilities to have notifications with email and/or sms. But it was unclear if it was activated/implemented.


Have a nice day.
96
Telematics / Notifications
« Last post by FluidPowerTom on June 16, 2021, 08:46:54 PM »
Do push notifications or alarms or whatever work currently, and are they functional with the CS100?  I'm trying to sort out how to make my CS100 send email or text notifications based on data it receives.  The Notifications section of the CONNECT portal seems unclear on how to do this.

EDIT:  We figured it out.  It doesn't appear to be documented anywhere or even shown in any of the CAB stuff though.  So, the Notifications in the wheel drop down in the upper right is different than the Notifications you can click on the left.  The former is for creating notifications.  It'd be good to name it as such.

EDIT 2:  Can it not send a text message?
97
Telematics / Dashboard and Configuration Feedback
« Last post by FluidPowerTom on June 15, 2021, 11:12:23 PM »
Nice work Danfoss!  The configuration was very smooth and easy.  The copy/clone feature is a spectacular time saver.  This is definitely a product that we can work with and sell.  Better late than never.

As a side note I see that we have the ability to add gauges and charts.  Does the display team know about these features? 
98
General controls / Re: Code compare
« Last post by G30RG3 on June 14, 2021, 01:30:36 PM »
For this tool you need an Add-on License: https://assets.danfoss.com/documents/79120/AI170686484256en-000205.pdf
In Text based programming languages code versions can be compared for free :) Just saying.
99
General controls / Re: Code compare
« Last post by Tor on June 14, 2021, 07:20:04 AM »
Hello,

In PLUS+1 GUIDE you have the Support Tool called Compare SCS.  Search for "Compare SCS" in the User Manual and read more about it. https://assets.danfoss.com/documents/161209/AQ152886483724en-002301.pdf
For this tool you need an Add-on License: https://assets.danfoss.com/documents/79120/AI170686484256en-000205.pdf

Have a nice day.
100
General controls / Code compare
« Last post by swordfeather on June 13, 2021, 04:06:58 PM »
Hi,

Does anyone have some tips/tricks for code compare between two versions?
For now i export the complete code to one page which I insert in the new version and switch back and forth between the two.

Any guide tools for this?

Thx in advance.

Pages: 1 ... 8 9 [10]