Recent Posts

Pages: [1] 2 3 ... 10
1
Function Library / PID function block weirdness?
« Last post by G30RG3 on July 30, 2021, 06:48:01 PM »
Hi all,

I've got a stability issue with a PID speed control.
I'm trying to use a PI or PID Function block, v4.0 and Ive got some weird behavior:
When I disable the I- and D-functionality by setting the gains at 0, The I still rises when I change a speed set-point from 0.
By using the I-stop I'm able to cut that.  So the I-output and D-Output stay at 0, which is what I want.

But then I've got a next issue: Setting P-gain incrementally higher, results in my application getting stable up-to about 50% of the set-point, further increasing the P-gain, the control (P-Output) starts to oscillate wildly, without the error ever going negative. I would expect an oscillation to start once the Feedback goes over the setpoint, but I'm seeing this way before the first peak-value reaches set-point.

Any Ideas why the P-output behaves so weird?  I don't think there is an issue with overflows on my end of the programming, but a lot of the FB is hidden...
2
Off topic / ?? ?????? ?? ???????? ?????
« Last post by Sicfpglast on July 29, 2021, 03:04:53 AM »
???????????? ?? ??????
Tegs: ?????? ?????? https://signprint24.ru/
 
?? ?????? ?? ????????
?? ?????? ?? ??????
?? ?????? ?? ?????????? ?????????
3
Telematics / Configurations sometimes not all showing up on PLUS1 CONNECT
« Last post by FluidPowerTom on July 28, 2021, 08:32:27 PM »
Title says it all.  I thought I was crazy the first time it happened or that I'd accidentally deleted my latest Configuration version, but now it's happening again.  Then some days later when I logged in the version I thought had disappeared was back. 

This morning I was able to see all of the several versions of this Configuration I made, and for some reason right now I can only see a few of them.

EDIT:  What I've learned is that some of the configuration versions only show up in the Danfoss default group.  Why would only versions 4, 5, and 7 show up in the customer's subgroup but all versions up through 8 show up in the default group?  I could be mistaken, but I think they were all made in the subgroup.
4
Telematics / PLUS1 CONNECT J1939 Signal Library
« Last post by FluidPowerTom on July 27, 2021, 11:30:24 PM »
It looks like the SPN's from DM01 are not in the J1939 library as I go through the fairly exhaustive list of signals that are in there.  I guess there must be a reason for this, but I don't know what it is.  Is there a reason?
5
Telematics / Reports on PLUS1 CONNECT
« Last post by FluidPowerTom on July 27, 2021, 11:14:42 PM »
There is an issue that the 'Reports' area on the left side of the portal is only visible when you're connected to the Danfoss Default Group.  As a result of this basically customers cannot set up reports.  This needs to be fixed soon.
6
Off topic / ?? ?????? ?? ???? ?????
« Last post by Sicfpglast on July 27, 2021, 08:05:40 PM »
7
Displays / Re: DP710 - no images but everything else seems to work [RESOLVED]
« Last post by dlewis on July 26, 2021, 09:06:56 PM »
I do keep my files up to date via update center.  The issue was this was a program that has been in place for several years. I don't update old programs when new hardware files are released.  Too many programs out there to do this unless it's required.  In this particular case I needed to update 11 programs.

Was there a PIB that covered this issue?
9
PLUS+1™ Telematics Hardware / Re: CS500 Status
« Last post by Tor on July 23, 2021, 09:57:34 AM »
Hi FluidPowerTom,

That was my expectation as well. But since it's vacation time i can't get any information on this subject.
I hope it will be revealed what is happening next week.

Have a nice day
10
Off topic / Re: Como se llamo esto
« Last post by Tor on July 23, 2021, 08:00:28 AM »
Hi FluidPowerTom,

Missed one then.
The last month,or two, there have been a radical increase of "spam" accounts trying to get access. Sometimes one gets through the net.
I will remove his post, and account.

Thanks for letting us know.
Pages: [1] 2 3 ... 10