PLUS+1 User Forum

PLUS+1 Software => Displays => Topic started by: Camox on September 23, 2022, 12:12:45 PM

Title: DM1000 does not start
Post by: Camox on September 23, 2022, 12:12:45 PM
Hello,
I work with an DM1000 on my desk with a 24v power supply.
Today, the screen does not start. I verify the supply is good on C1P1 and C1P2.

I went through the documentation but I can’t find anything to check or test.
Do you have any idea?

Thank in advance.
Good day
Title: Re: DM1000 does not start
Post by: mtrbib on September 23, 2022, 01:42:31 PM
Hi,

Did you check if you are working with the newest HWD?

Can you still connect to it with the ServiceTool?

Best regards
Title: Re: DM1000 does not start
Post by: Camox on September 24, 2022, 08:20:08 AM
Hello,
Thanks four your response.
Ican't connect to the dysplay with the service tool.
I had updated the hardware file three weeks ago.

Thanks
Title: Re: DM1000 does not start
Post by: deaks57 on September 26, 2022, 12:39:22 AM
Contact Danfoss. There is a way to fix this.
Title: Re: DM1000 does not start
Post by: ramzilla on October 10, 2022, 05:35:10 PM
I had to add a switch on the power wire in order to get a DM1000 to power up with a desktop power supply. Turning on the power supply would not power up the display. I have to turn on the power supply and then flip the switch to get it to come on.
Title: Re: DM1000 does not start
Post by: Camox on October 12, 2022, 11:48:19 AM
Yes. Thanks.
I think is this problem.
I have also a mystake with my wire.