PLUS+1 User Forum

PLUS+1 Hardware => Controllers => Topic started by: TheTurfDude on March 08, 2019, 07:37:43 PM

Title: Danfoss MC and Load cell
Post by: TheTurfDude on March 08, 2019, 07:37:43 PM
Has anyone successfully used a Danfoss Micro to measure an input from a load cell? The load cell in question is an Omega LC101-5K. The output from the Wheatstone bridge circuit is a very small mV signal and I am not sure how this can be read with a Danfoss controller. We are using an MC050-110.

Would an amplifier do the trick? Just curious if this has been done already and if so, what advice someone may have.
Title: Re: Danfoss MC and Load cell
Post by: jashom1 on March 11, 2019, 10:52:49 PM
Hi,

Have you seen this thread?

http://www.plus1forum.danfoss.com/index.php?topic=879.msg2672#msg2672 (http://www.plus1forum.danfoss.com/index.php?topic=879.msg2672#msg2672)

I haven't used them but they should work.

Cheers,

John.
Title: Re: Danfoss MC and Load cell
Post by: TheTurfDude on March 12, 2019, 03:17:57 PM
I did not see that thread. Thanks John.