PLUS+1 User Forum

PLUS+1™ Tools => PLUS+1™ GUIDE CANKing => Topic started by: Jerry B on August 27, 2018, 06:24:01 PM

Title: CAN Channel - "Can not find the CAN driver!"
Post by: Jerry B on August 27, 2018, 06:24:01 PM
Under the Bus Parameters tab, CAN Channel is greyed out and reading "Can not find the CAN driver!". Anyone know how to point CanKing to the CG150 drivers? The drivers are showing up for the Service tool. Any help in getting CanKing to work is greatly appreciated.
Title: Re: CAN Channel - "Can not find the CAN driver!"
Post by: Jerry B on August 27, 2018, 10:14:47 PM
I was able to fix the issue by updating the firmware on the CG150 cable. Then I uninstalled and re-installed the CanKing software. The CG150 cable along with 2 virtual connections are now available under the Bus Parameters tab>CAN Channel.

I also had the issue of the wc32.exe error when opening the program. Setting the wc32.exe to always run as admin fixed that issue.