PLUS+1 Hardware > Controllers
output shared
(1/1)
topal:
Hi,
I've been looking for a while and couldn't find it so I'm posting here
I need to share an output from my MC50 controller but it doesn't work because as soon as this output is already wired, it gives me an error when compiling
in my application I have to control 3 distributors, one of which is common regardless of the distributor used
Is there a software solution to my problem because setting a go pair two outputs I only see that!
thank you
Pat
FluidPowerTom:
Are you wanting to use the output for 2 possible different functions depending on the type of machine or something like that? If so you can use a boolean switch or value connect to change what logic controls the output.
topal:
Hello,
i used this way and it works
thank you
Pat
Navigation
[0] Message Index
Go to full version