PLUS+1 Hardware > PLUS+1 Compliant Hardware
PRESSURE SENSOR BLOCK
(1/1)
pinias:
Just for the record,
the signals name for pin configuration changed on the MC050-120, if I want to use a Sensor Block, it just does not work, trying to guess what I have to disconnect BIAS or RANGE , no luck, the compilation throws an error.
the manual for the sensor is based on the old signal names and it seems that the lastest revision of the blocks is the 1.00 or at least is the one I can get from the download center.
I did my own firmware for that but I wonder why the Danfoss do not work, I use to use them with all the MC050-010, 110, MC012, and displays without any issue.
Regards
Navigation
[0] Message Index
Go to full version