Author Topic: Can isolation  (Read 19075 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 131
  • Karma: +1/-0
Can isolation
« on: February 01, 2024, 03:28:48 PM »
Hello all,

I use module SC050, OX024, DM430 and engine
I want to use Can_0 communication only between SC050 and engine.
And use Can_1 communication with SC050, OX024 and DM430.
I think for module OX024 it's ok.  It's done Please see image enclosed.
But I don't know if I must to change also Can_0 of DM430 and SC050 secondary to Can_1.
Or just connecting modules to Can_Bus_1.
Specially SC050 secondary.

I hope you understand my idea.

Thanks in advance for you help

With best regards
Mac bahi


Offline mtrbib

  • PLUS+1 User
  • **
  • Posts: 9
  • Karma: +1/-0
Re: Can isolation
« Reply #1 on: February 02, 2024, 03:47:21 PM »
Hello 8)

SC050:
- For the engine communicatione you need to use CAN0 (CAN port 0)
- For the OX024 and DM430 CAN1 (CAN port 1)

DM430:
- CAN0 (if you are using the physical CAN0)

OX024:
-CAN0

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 131
  • Karma: +1/-0
Re: Can isolation
« Reply #2 on: February 05, 2024, 11:20:01 PM »
Hello mtrbib

thanks

with best regards