Author Topic: MEDIA REPOSITORY  (Read 12811 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
MEDIA REPOSITORY
« on: December 12, 2020, 06:39:52 PM »
Hello Guys,

I have a need to include a PDF file in a DM1000, I have watched the youtube video to teach myself how to do it.

however there is something that I cannot do.

at minute 1:47 the danfoss guy access the Project Manager then Screen and application log repository after that he has a folder called MEDIA REPOSITORY

on this folder he is able to get the path for the file.

So in my case the Media repository folder does not exists yet, If I try to add a new repository that function is not enabled, see picture

does anyone know if that is a hardware issue or I had to configre something else first?

Thanks

Offline arned

  • PLUS+1 Novice
  • *
  • Posts: 4
  • Karma: +1/-0
Re: MEDIA REPOSITORY
« Reply #1 on: December 12, 2020, 08:29:08 PM »
Hi, to add a media file you will need to upgrade to a newer version of Guide. I've had this too...

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
Re: MEDIA REPOSITORY
« Reply #2 on: December 14, 2020, 03:33:06 PM »
yep that works

thanks buddy