Author Topic: Screen Editor - Unable to save index #  (Read 5116 times)

Offline THLL

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
Screen Editor - Unable to save index #
« on: July 05, 2018, 08:48:17 PM »
Using Screen Editor and creating a Text List on the Screen Manger side I am unable to keep an assigned text index to a number. The list gets assigned to a Active Index Signal so if I get a "23" as my signal the text index assigned to "23" should display.

However when I do assign a "23" to a text index, save, compile, close, then reopen the index number gets reverted back to whatever sequential order it was in. Why doesn't the assigned index number save? 

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Screen Editor - Unable to save index #
« Reply #1 on: July 11, 2018, 07:30:14 AM »
Which Text editor is it? Classic or vector based (DP700,...).
Could you post some pictures ?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung