Author Topic: CAN0 R and L in DP610LX  (Read 6027 times)

Offline Federico

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +1/-0
    • Centro Hidráulico S. A.
CAN0 R and L in DP610LX
« on: August 16, 2013, 04:39:13 PM »
Estimados, alguno podría indicarme cuales son las diferencias entre CAN R y CAN L?

Necesito comandar 2 motores Diesel y pienso utilizar un CAN0 para cada uno, el tráfico es independiente? La carga del Bus es la suma de cada carga?

Saludos
**************************************

Dear, someone could tell me what are the differences between "CAN0 R" and "CAN0 L"?

I need to commandeer two diesel engines and I use a CAN0 for each. Traffic is independent? The bus load is the sum of both load?

regards

Randy

  • Guest
Re: CAN0 R and L in DP610LX
« Reply #1 on: August 16, 2013, 07:25:23 PM »
Hello Federico,

The CAN0 R and CAN0 L are related to the REDCAN feature.
The software provides an interface to be able to use either pin set or both pin sets depending on the mode/configuration.
Both sets of pins can get connected to the same CAN0 Transciever, again depending on the mode/configuration.
If it is configured to use both sets of pins, they are effectively on the same bus and traffic is not independent.

I hope this helps.

Randy