PLUS+1 Hardware > PLUS+1 Compliant Hardware

PVED-CC S7 ISOBUS when CAN network is down.

(1/1)

jert:
I have had a failure with our Danfoss PVED-CC S7 valves when the CAN network fails. If the valve was commanded on it keeps going even though the CAN network is down.  Is there a parameter that I can set so that if the valve loses the CAN signal it will stop immediately or go to neutral?

G30RG3:
AFAIK the PVE should generate an error after 250ms.
I guess you've set the fault monitoring to passive?
Setting this to active, should bring the PVE to a safe state in case of an error.

Navigation

[0] Message Index

Go to full version