Author Topic: Controller with no I/O  (Read 1463 times)

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Controller with no I/O
« on: April 06, 2023, 08:25:24 PM »
I've been asked by a larger customer of ours if there's a small controller with little or zero I/O that has two independent CAN bus ports.  They need the two CAN ports, but all of their I/O are CAN devices.  Is anything in the works that is smaller than a MC024 and has two CAN buses?
Controls Engineer
Hydra-Power Systems

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 278
  • Karma: +27/-1
Re: Controller with no I/O
« Reply #1 on: April 12, 2023, 11:43:20 AM »
Hello,

I hope you don't mind that I moved it to the "Controllers" topic instead.

A small controller with minimum I/O and two CAN bus ports.
The only one that I can think of and fits that description is the DM430 with dual CAN.  But I guess there's the small question about cost as well.
Have I forgot something? Maybe someone else knows?

Sorry that I didn't have a better answer.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: Controller with no I/O
« Reply #2 on: April 12, 2023, 05:13:08 PM »
Indeed the DM430 actually costs more than the smallest controller with 2 CAN ports (MC024).  As you might imagine the cost is really the driving factor, and it seems like I/O - especially outputs - are generally a driving force behind price.
Controls Engineer
Hydra-Power Systems

Offline Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +5/-0
Re: Controller with no I/O
« Reply #3 on: April 14, 2023, 01:28:40 AM »
Tom out of curiosity what exact model/number MC024 has 2 CAN ports? I thought it only had 1 port.
I know the MC050 has 2 ports.

Offline G30RG3

  • PLUS+1 Expert
  • ****
  • Posts: 71
  • Karma: +3/-0
Re: Controller with no I/O
« Reply #4 on: April 14, 2023, 08:24:42 AM »
That would be the MC024-130 (11144803) or MC024-132 (11144804)