PLUS+1 User Forum
PLUS+1 Software => General controls => Topic started by: Earthmover on February 15, 2013, 11:35:25 PM
-
Hi - this is not necessarily a PLUS+1 question per se but I need some help with controlling a 12V PVEM as a newbie.
We have 12v type 157B4116 PVEM's with Hirschmans which we wish to use as bi-directional proportional control on a motor. We are using ethernet controlled digital to analogue outputs rather than Plus+1 stuff as we have a very particular requirement.
Electrically we have 12 V (U+) on Pin 1, an Earth and the control/proportional signal on Pin 2. This would map to Prop2/US2 on a Sauer controller. The set up is the same as the minimum safety electrical diagram you see in the PVG pdf documents.
My expectation that was that a control signal of 6v would put the valve in a closed neutral position. A signal of 3 to <6v would run fluid one way and >6v to 9V the other way. The problem is that only the >6v to 9v signal works and sends fluid one way only. Nothing happens with a <6V signal. The wiring diagrams are not that clear (to me).
Can anyone tell me what I've missed or offer a troubleshooter? The diagrams do show a separate signal line onto Pin1 coming from N_SW-Out. What does this do and should we be using it?
thanks - I'm desperate as we're supposed to have a system test Monday!
-
Hello,
This may be a little delayed, however I believe you need to use three pins on the PVEM Hirschmann Coils.
1 for Supply Voltagee
1 for Control Voltage
1 for earth ground
Did you have proportional control of the one direction that is properly worked?
I will try and help any way I can.
I am a newbie too.. so I know the feeling.
Cheers!
-
Are you sure the valve is not expecting 24 volts?
-
Hi,
1. 157B4116 is PVEM, 12V (11..15V)
2. Be care to use PWM Output. PVEM needs analog signals.
We have adapters 0..10V or 4..20mA to Sauer - dAnfoss 25..75% (10..30V)
I think this is not your problem, but please only use analog signals.
Please measure the signals.
3. Maybe the problem is a hydraulic problem, pilot oil.....?
For new pojects I would use PVEA.
Best regards,
Bernd