Author Topic: New SC controller?  (Read 4489 times)

Offline Loader

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +3/-0
  • If something can go wrong, it will!
New SC controller?
« on: February 22, 2019, 11:11:22 AM »
Hi,
Does Danfoss have in mind to produce a SC controller with more than 50 pins and with more current inputs?
It would be great!
Thanks

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: New SC controller?
« Reply #1 on: March 15, 2019, 01:31:48 PM »
Hi Loader!

It has taken a while to get the information but now we can present there will be a XL/full controller! The XL controller is a power house employing a 32bit Proces-sor, providing the controller with extremely fast single cycle processing speed and 2.5 MB of internal flash. The architecture of the XL controller platform furthermore gives you the oppor-tunity to comply with current functional safety standards.Attached you can find a data sheet but remember, it's only a DRAFT!

Best regards
Nilla
PLUS+1 Helpdesk

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +2/-0
    • Trebro Turf Equipment
Re: New SC controller?
« Reply #2 on: March 20, 2019, 06:24:59 PM »
Any idea on projected release date?

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: New SC controller?
« Reply #3 on: March 21, 2019, 01:39:16 PM »
Hi all!

Early 2020 is all I got.

Best regards
Nilla
PLUS+1 Helpdesk team