PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: Nick Anderson on January 18, 2017, 08:26:40 PM
-
Has anybody investigated whether a controller's address can be updated dynamically in real-time. I was configuring a couple I/O modules and was thinking that if we're dynamically changing the address of the I/O module during configuration, can we do the same thing with a controller? I tried to make a file that would set the address based on encoding 4 separate inputs, but kept getting an error saying the node address init component has to be connected to the output of something that can be set at initialization.
-
A Non-volatile memory component has an output that is set at initialization, so I use an external input or two to pick the address, and if it's different than what is stored I save it to NV memory. Here's an example from a DP700 project.