Recent Posts

Pages: 1 2 3 [4] 5 6 ... 10
31
Displays / Re: DM1000 ETHERNET
« Last post by Lukey on February 21, 2025, 01:32:22 AM »
EXPERIMENTAL annotation fills me with great confidence... makes me all warm and fuzzy, yay
32
Displays / Re: DM1000 ETHERNET
« Last post by Beezkneez on February 20, 2025, 10:12:10 PM »
In case anyone else is interested in using the ethernet interface on the DM series displays, I received a reply from helpdesk on how to test. There were actually examples already in the hardware tab, I just did not look there. I will attach the screenshot on where to find the examples for TCP/UDP.

33
PLUS+1 GUIDE / Urgent Plus+1 Guide Screen Editor Problem
« Last post by macbahi on February 19, 2025, 02:36:53 PM »
Hello,

I use Plus+1 guide version 2024.3.5.  When I use screen Editor,  I can't see all elements added in folder Screen manager as shown in image below.

Thank you very much for your help.

With best regards.

mac bahi
34
PLUS+1 GUIDE / Re: Plus+1 Guide Horizontal&vertical bar modification
« Last post by macbahi on February 18, 2025, 04:21:54 PM »
Thanks Lukey for this information.

With best regards
35
PLUS+1 GUIDE / Re: Plus+1 Guide Horizontal&vertical bar modification
« Last post by Lukey on February 18, 2025, 01:42:45 AM »
It cannot be changed, I've already contacted the help desk about this, apparently it is in the pipeline for development but with no immediate due date.
36
PLUS+1 GUIDE / Plus+1 Guide Horizontal&vertical bar modification
« Last post by macbahi on February 17, 2025, 04:30:13 PM »
Hello,

I installed a new Plus+1 guide version 2024.3.5.  But I didn't like the vertical icon tool bar position?  Please See image enclosed?

Please Could you tell me a way to change the vertical icon tool bar to horizontal?

Thank you very much.

With best regards.

mac bahi
37
Displays / Re: DM1000 ETHERNET
« Last post by Beezkneez on February 06, 2025, 04:12:14 PM »
Hi Tor,

Thanks for the response. I have had an open ticket with helpdesk about this for a few days. Have not heard anything and that is why I posted in the forum.

I am aware of the ethernet output page and how to enable the interface, but how do I use it?

Where do I configure messages or packets to be sent and received and then used within PLUS+1 code? I would like to be able to send/receive data on the ethernet interface and I have not seen anywhere on how to do that with PLUS+1.

What protocols are available on the ethernet interface?

Thanks.
38
Displays / Re: DM1000 ETHERNET
« Last post by Tor on February 06, 2025, 09:09:20 AM »
Hello,

As far as I know Ethernet should work on the DM1000 and some models of the DM700.
What I understand you have to enable it in the template. In the outputs page there is a Ethernet page, and the enable signal needs to be set to True.

If you don't get it to work, please contact PLUS+1 Helpdesk: https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-support


Have a nice day.
39
Displays / Re: DM1000 ETHERNET
« Last post by Beezkneez on February 05, 2025, 05:02:35 PM »
Any updates on this?

I too would like to use the ethernet interface to communicate with other IP devices. I have not seen anything in documentation on how to achieve this.

Has anyone gotten any info from Danfoss or had any success doing this?
40
PLUS+1 GUIDE / Re: error 65 on CAN open PDO_Rx
« Last post by llang on January 30, 2025, 07:09:54 AM »
Hi Camox,

i'm sorry for the late answer. This was exactly the problem, thanks a lot!
Pages: 1 2 3 [4] 5 6 ... 10