Hello Stefan,
look, I need to get clutch RPMS, so I installed a KKPG16708 PICK UP SENSOR. I am using a MC050-10 controller and I am using PIN 18 for inpit of the pick up sensor.
the picture attached shows the pin config and the way the freq to rpm block is connected. I understand in thsi way it should work or I should be able to read RPM, however I read nothing.
what could I be doing wrong?
My system is 24VDC.
this is the fisrt time I am using a pick up with the PLUS 1 so no too much idea what could be wrong int he firmware.
I have tried other advises posted in this fórum but so far no luck
I appreciate any feedback on this
Thanks