Recent Posts

Pages: 1 [2] 3 4 ... 10
11
PLUS+1 CS Hardware / Re: CS500 GUIDE Intergration / Function Block ?
« Last post by Lukey on December 03, 2023, 04:38:30 AM »
Danfoss support was unable to provide a change log but have been very helpful otherwise.

Yes I recommend waiting till v116 if you're wanting to send GNSS data over the CAN bus.
12
PLUS+1 GUIDE / Re: Input hexadecimal???
« Last post by sverreo on December 01, 2023, 09:28:52 PM »
Cheers acmall, i didn't know it was there :)

I tested it a bit, and it seems i need to make some logic if the first decimal after the point (right side) is "0", then it gets lost in this function and the first decimal >0 is displayed...
13
Displays / color-grafic as watermark possible?
« Last post by Marbek_Elektronik on December 01, 2023, 09:02:32 PM »
Hello,
my customer wants pictures transparent behind other elements, other pictures.
Is this possible for example by DP700, vector graphics?

can I change anything on a color picture exept position and ratio?
can I change transparent or any color or x,y dimensions? I think not.

Thanks.
14
PLUS+1 CS Hardware / Re: CS500 GUIDE Intergration / Function Block ?
« Last post by mvanwiechen on December 01, 2023, 04:20:20 PM »
I was wondering the same, regarding update log for a new version of the firmware.

I'm not sure if it is worth my time to update to v115, or if I should just wait to v116.
15
PLUS+1 CS Hardware / Re: CS500 GUIDE Intergration / Function Block ?
« Last post by Camox on December 01, 2023, 02:04:07 PM »
Quote
Anyone know where an update/fix log for v115 firmware can be found/downloaded?

I don't know if this information is provided by Danfoss.

Have you asked support?
16
PLUS+1 GUIDE / Re: Input hexadecimal???
« Last post by acmall on December 01, 2023, 08:54:40 AM »
There is a block in the Utility FB Library called IEEE_754 which it states is for converting from IEEE_745 floating point representation to a fixed point notation if that helps.

You can install the Library from the Plus+1 Update Centre where it is listed as Utility Library 70380479
17
PLUS+1 GUIDE / Re: Input hexadecimal???
« Last post by sverreo on November 30, 2023, 11:22:15 PM »
Dose anyone have the "float multiply block" that @jashom1 posted an image of in this thread?
18
PLUS+1 CS Hardware / Re: CS500 GUIDE Intergration / Function Block ?
« Last post by Lukey on November 30, 2023, 03:15:11 AM »
I can confirm v115 release has not fixed the GNSS messaging over CAN via Virtual Signal Triggers or Periodically timers.

Fingers crossed for imminent v116 release fix.

Anyone know where an update/fix log for v115 firmware can be found/downloaded?
19
Displays / Re: Lifetime NVmem Erase/Write for DM430E
« Last post by Marbek_Elektronik on November 29, 2023, 04:12:54 PM »
Normally this EEproms are ferromagnetic and so millions of erase/write cycles.
I just find no document, sorry.
20
Displays / Re: Draw lines and points
« Last post by Marbek_Elektronik on November 29, 2023, 03:23:04 PM »
I will do (next weeks) a x-y-graph on a DM430E.
I want to vary parameters and then see how the graph changes.
I hope this works.
Then I'll post it if it helps.
Of course, there are a lot of points and every point has to set per value.
Pages: 1 [2] 3 4 ... 10