Hello,
I am trying to use the Danfoss 40 series and 90 series pump control function blocks to control EDC's for hydraulic functions. I'm using a J1939 joystick as the input device. When I manipulate the joystick, I can measure a small output on the relevant wires for roughly 1/2 second, then the output immediately drops to zero and stays there until I power cycle the controller. After a power cycle, I get the same 1/2 second of output, then zero again.
I feel like this must be caused by some fault detection either within the function block or the controller itself. I have disabled fault detection in the function block by changing the boolean FltDet value to false. I'm not sure what else could be causing this. I came in this morning hoping that I could use the fault manager function block to determine what type of error is causing this behavior, but when I started reading the documentation for the fault manager, I started to suspect that this function block is for something much more complex. I'm not trying to set up custom faults. I just need to figure out why my controller is cutting off output to my pump EDC's. If anybody has advice on the quickest and simplest way to figure this out, I would be extremely appreciative.
Thank you in advance.
Robbie