Author Topic: 2nd machine  (Read 17440 times)

Offline Undertow

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +0/-0
2nd machine
« on: January 20, 2011, 10:17:27 AM »
Hi,
Can anyone explain how I add a license to my 2nd computer?

Thanks

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 72
  • Karma: +0/-0
Re: 2nd machine
« Reply #1 on: January 20, 2011, 11:23:31 AM »
Hello,

Put in the license key you got for the first PC into License Manager and click on Rehost. Send the email and then you will receive a license key for the second PC.

Best regards
Stefan

paterianus

  • Guest
Re: 2nd machine
« Reply #2 on: May 11, 2011, 04:32:37 PM »
Will this allow me to have activations on both systems simultaneously, i.e. desktop and laptop?

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 72
  • Karma: +0/-0
Re: 2nd machine
« Reply #3 on: May 11, 2011, 05:12:46 PM »
Hello,

Yes, it will.

Best regards
Stefan

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: 2nd machine
« Reply #4 on: October 03, 2016, 08:39:06 AM »
Very good,
because it is not possible to open 2 times Guide at one computer.
I have to work with two programs simultaneously

So I use 2 computers and run Guide on both computers at the same time.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: 2nd machine
« Reply #5 on: October 12, 2016, 11:08:48 AM »
Hi Marbek!

Don't forget that you have the Module viewer option under View in the menu. This window provides an additional window, independent of the main PLUS+1 GUIDE window, in which you can edit SCS files. Typical uses of this window include:

  • Seeing multiple pages within the same project. (You can open the SCS file for your current project in this window.)
  • Coordinating CAN communications between two controllers
  • Copying parts of code from one project to another

You can read more about it on page 205 in the GUIDE User Manual 10100824 Rev 1401 from February 2016 found on our website.

Best regards
Nilla
PLUS+1 Helpdesk team

Offline Chris W

  • PLUS+1 Developer
  • ***
  • Posts: 16
  • Karma: +4/-0
Re: 2nd machine
« Reply #6 on: October 12, 2016, 05:20:23 PM »
Sneak peek!

We're getting close to our 9.0 release, which is currently scheduled for late October.  In this release, the Module Viewer is being transitioned to a stand-alone tool.  This will allow you to associate SCS files in Windows with the Module Viewer and allow you to open up multiple instance.  This will be very useful since it can open faster than GUIDE and now you can open the SCS files directly from your project directories in Windows.

Additionally, the same is true for the SCS Compare Tool (outside US only)!  We'll post an update once the new version is available!

Best Regards,

Chris
Danfoss Power Solutions
Product Application Engineer

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: 2nd machine
« Reply #7 on: November 07, 2016, 02:12:58 PM »
@Nilla: yes, module viewer is very nice, but can't open screens.......
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung