Author Topic: Sick S100 laser  (Read 16118 times)

paterianus

  • Guest
Sick S100 laser
« on: November 04, 2011, 09:46:15 PM »
The Sick unit states as noted below that its CAN compliant.  I dont see these standards referenced within the S-D documentation.  Can I interface the unit to a plus+1 controller?

CANopen as per the CiA standards DS301 and DS401. The S100 represents a so-called SDO server, is a SYNC consumer, an NMT slave and supports a PDO with a CAN message with 8 bytes of useful data in each transmission direction.

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 74
  • Karma: +1/-0
Re: Sick S100 laser
« Reply #1 on: November 09, 2011, 08:44:01 AM »
Hello,

In the attached pdf you can find some basic information about CANopen. I hope that will help you to program GUIDE.

Best regards
Stefan