Author Topic: Text List superimposed with there line background  (Read 3395 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 115
  • Karma: +1/-0
Text List superimposed with there line background
« on: December 20, 2022, 10:24:58 PM »
Hello,

I use 4 Text-List with their bottom line in different color. They are all superimposed (one above the other). They will appear following logical conditions (their enable). Sometimes it can happen that two or three Text Lists are activated at the same time. For this reason I applied priority to each. 0,1,2,3 as mentioned in the document the high priority is 0 and lower priority is 4.
But unfortunately I only see text list priority 0.
Please could you correct me if I'm getting confused.
I had using a second method using Image List for only the 4 background lines creating there 4 different background color images. But unfortunately I can't change the width or height independently of Image List. Each image is 304x72.
If I change Image List's width the Height also changes automatically and vice versa.

Thanks for your help
With best regards