PLUS+1 Tools > PLUS+1 Service Tool
Image repository directory not found.
Fredrick:
Hi,
When trying to save a P1D file in ServiceTool 2022.2.5 I get the message "Image repository directory not found." and if I click Yes all images that are in the P1D file disapears.
Even if I manualy add them again I will get the same question again when trying to save the P1D file.
Please se the attached picture.
Fredrick:
Anyone else having problems with this?
Also, sometimes the P1D file does´t get saved so next time you open the P1D file the changes are lost and you now have an older P1D file without the changes you just did. :(
Tor:
Hello,
This issue is reported (P100006351) and will be fixed in the next release.
I recommend to use the 2022.1 until this is fixed.
Sorry about the inconvenience.
Fredrick:
Thank you for the information. :)
Fredrick:
ServiceTool 2022.2.6 fixed the issue with the "Image repository directory not found." when using "File/Save As" in ServiceTool
But the problem is still present when importing some PFX files in ServiceTool, I get the same error message after I have imported a PFX file into the Tool and then trys to save.
In 2022.1 it works when I try to do the same action.
Navigation
[0] Message Index
[#] Next page
Go to full version