Author Topic: IEEEC 754 into Plus+1  (Read 4216 times)

Ebby

  • Guest
IEEEC 754 into Plus+1
« on: January 17, 2017, 06:54:32 AM »
Attatched is a brief description of our problem in a word doc
Any help or advise is much appreciated

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: IEEEC 754 into Plus+1
« Reply #1 on: January 18, 2017, 02:01:31 AM »
This looks like the same problem you are dealing with in another thread:

http://www.plus1forum.danfoss.com/index.php?topic=974.0

« Last Edit: January 18, 2017, 02:03:46 AM by oiltronic »

Offline ZanInno

  • PLUS+1 Developer
  • ***
  • Posts: 17
  • Karma: +3/-0
Re: IEEEC 754 into Plus+1
« Reply #2 on: January 19, 2017, 01:20:10 PM »
I have worked with the Mantra load cell cards in the past.  The output can be converted to a 32 bit integer with a gain of 1,000,000.  The value can then be read directly into the +1 without converting from a floating format.