Author Topic: How to create a chart using 2 array lists checkpoints  (Read 4928 times)

Offline Loader

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +3/-0
  • If something can go wrong, it will!
How to create a chart using 2 array lists checkpoints
« on: January 19, 2017, 02:32:12 PM »
Hi everybody!
I need to create a chart, using the elements of two array lists checkpoints.
Right now I log to file and then I copy and paste the values in a Excel file.
Is there a way to copy the numbers directly from the Service Tool page, or to create the chart inside the tool?
Thank you!
Best regards