PLUS+1 Tools > PLUS+1 Service Tool
ERROR: 260
(1/1)
briandyck:
I am in the process of trying to remotely download to a controller. System connects and scans fine. Existing program works great - Just need to download an interlock to an existing function. The problem occurs as I start to download. Get error code
"Unable to write ECU History"
Error: 260
Function Download File
Any suggestions
briandyck:
Got it!
The guys in the shop out there were leaving for the night and thus hooked up a battery charger to the unit so that we could leave power on until I got it working.
As soon as the charger was hooked up the very next download attempt completed. Must've been too low battery voltage I am guessing to program correctly??
At any rate - looks like if you see an Error: 260 check your battery voltage...... ;)
Brian
jmerson:
are you familiar with error 1? Low value for Y axis?
briandyck:
I am assuming that you are getting this as a compile error? Are you using the "Manage" Generate Compiler Error on Range component? I have pasted the info from the help guide below....hopefully this helps.
Generate Compiler Error on Range
Use:
· Aborts the compile process when the compiler finds an out-of-range constant value
· Displays a user-defined error message in the Error Messages tab
· Prevents a user from entering a value that compiles but causes erratic operation when downloaded
(For example, a joystick calibration value that is too high would compile successfully but might cause erratic machine operation when downloaded
Function:
· A1 = Constant value
· Low? = Click with Query/Change to enter the low value for the range
· High? = Click with Query/Change to enter the high value for the range
· MSG? = Click with Query/Change to enter the error message that displays if A1 is out of range
Navigation
[0] Message Index
Go to full version