Author Topic: DM430E - Bricked  (Read 1333 times)

Offline george

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
DM430E - Bricked
« on: November 04, 2024, 03:07:51 PM »
Hi,

We bought two DM430E 0-0-0-0 displays and one of them is bricked on flashing the test application.
The application flashed successfully and the GUI has changed as expected.
However the display is neither sending CAN messages nor recognised in "Recover ECU" for reflashing.
Looks like it is bricked.

We are using PCAN View, with RP1210C interface.
Could you please help to resolve this?

Service tool version is: 2024.2.5.6053

Offline george

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: DM430E - Bricked
« Reply #1 on: November 05, 2024, 11:18:46 AM »
Any thoughts?
This is a stopping issue and I am unable to get it resolved.
Is there any technical team I can talk to or an email where I can email the issue further?
Thanks.

Offline george

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: DM430E - Bricked
« Reply #2 on: November 05, 2024, 12:01:02 PM »
I tried to access the command line mode and got the following log. Still the download is failed.

PLUS+1 Service Tool 2024.2.5
Running on supported OS Windows 11_64
Copyright © 2004-2024 Danfoss All Rights Reserved

68339578

    Verifying installation...

68342703

    Loading user interface...

Loading user interface...
Changing to Online mode
Gateway: RP1210C: PEAK-System PCAN Adapter (PEAKRP32)
Channel: DeviceID 1: PEAK-System CAN Adapter (USB
Protocol initialization...
Baudrate: 500 kbit/s
Status:
Performing system scan...
System Scan result:
   ECU: 0,23
Result: ECU in boot loader mode. No valid application running.
Opening download package: C:\Git\Danfoss\Test_100\Test_100.lhx
Download File #1
Download: true
ECU: 0,23 - dm430e_display
FileType: Application
FileName: Test_100.lhx

ERROR: Unable to start File Download.

Offline george

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: DM430E - Bricked
« Reply #3 on: November 05, 2024, 12:44:22 PM »
As I have two units, and here is the log from the bricked unit. No heartbeat of CAN messages. Display screen comes back normal with the previously programmed screen.

PLUS+1 Service Tool 2024.2.5
Running on supported OS Windows 11_64
Copyright © 2004-2024 Danfoss All Rights Reserved

69326546

    Verifying installation...

69329687

    Loading user interface...

Loading user interface...
Changing to Online mode
Gateway: RP1210C: PEAK-System PCAN Adapter (PEAKRP32)
Channel: DeviceID 1: PEAK-System CAN Adapter (USB
Protocol initialization...
Baudrate: 500 kbit/s
Status:
Performing system scan...
System Scan result:
ERROR: No ECU information available.
A connected system is required.

Offline G30RG3

  • PLUS+1 Expert
  • ****
  • Posts: 75
  • Karma: +3/-0
Re: DM430E - Bricked
« Reply #4 on: November 05, 2024, 06:00:05 PM »
Are you sure you're on the right baud rate? You won't be able to communicate if your screen has switched to 125k, 250k, or 1M with a gateway set to 500k.

Offline Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 71
  • Karma: +8/-0
Re: DM430E - Bricked
« Reply #5 on: November 06, 2024, 01:00:14 AM »
G30RG3 maybe be right.

The default baud rate is 250kbps, possibly if the display has gone into bootloader and reset, its rate is now 250kbps.

Have you tired to recover the ECU? this will get it back to a state where you can download/flash a new lhx file.
Read page 36 onwards of the PLUS+1® Service Tool User Manual