Author Topic: RTC GNSS TIME updated  (Read 12472 times)

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 119
  • Karma: +0/-0
    • Dewind Dewatering
RTC GNSS TIME updated
« on: May 02, 2024, 09:39:56 PM »
I recently found out I can sync the DM1200 clock with GPS by just enabling GNSS and connecting a GPS receiver antenna. Now that I know that the time is perfect I wish to get info that it has indeed synced which according to the API I can use RTC.Auto, atleast I think I can, to light up an indicator. I need this to work with our Trimble GPS sytem for DATA logging and machine logging. I have a setup where the Danfoss computer trips a relay which acts like a button push on the Trimble system to create a point.

I cannot find on the RTC bus the .Auto element which the API says is there. Has anyone used this function or have an idea how to read the .Auto data?