Author Topic: CAN fault shutdown  (Read 4709 times)

paterianus

  • Guest
CAN fault shutdown
« on: January 31, 2011, 05:05:25 PM »
Is there a simple method of disabling outputs on a CAN bus fault?

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: CAN fault shutdown
« Reply #1 on: January 31, 2011, 08:07:08 PM »

You could use the message received flag in a CAN buffer in conjunction with a off delay, something similar to this should be used anyway as a matter of safety. If no message is received the switch resets to zero after 1 second.
Neil.