PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 GUIDE => Topic started by: LBee11 on May 16, 2017, 08:54:10 PM
-
Hi All, me again!
I'm trying to get my head around writing to a USB. I can write to a Log file in the HMI, but am struggling with the Read_Applog function.
Im currently getting the following error from the Read_Applog:
Line index overflow—the function block cannot find the line that contains the CSV record in
the controller’s application data log.
I'm also getting an error from the Write_USB block:
Error; record write not completed; the next program loop resets this bit.
I'm not sure where I'm going wrong, attached is the snippet i'm using (Only for testing!). I can't specify an index, so where is the error?
TIA
-
I got this working, found the help file that supports these two functions and wired it like the example shows. Works correctly after that!