PLUS+1 Software > Displays
Toggle between Screen Area Pages
bgtwuk:
Good Morning
I am new at this of course. I have two screen area pages, and am trying to select between them with a soft button.
I have an enable port for each page, that I believe should have the proper affect.
Am using a simple switch but my pages are not toggling properly.
The fog is thick up here eh!
Bgtwuk
Thomas:
Hi!
Have you connected your enabling signal inside the Area? It is very easy to forget.
Best regards // Thomas
bgtwuk:
Very Interesting.
I will try that.
Thanx
Marbek_Elektronik:
Hi,
I have another question about toggling area pages:
I have a program with very much area pages.
Now, I have to add a new area page which can be placed everytime and everywhere on display.
It is a "help-screen".
My question:
Is it OK to switch on this new area page and it will appear in front of all other areas?
If I switch off this help-menue it will disappear and the screen is as it was before this action.
Is there a rule like: The last area wins?
Daniel:
Hi Bernd
Yes that is correct.
And the last area of the enabled areas wins.
Best regards
Daniel
PLUS+1® HelpDesk
Navigation
[0] Message Index
[#] Next page
Go to full version