PLUS+1 Hardware > Controllers
use MC50 and IOX24 together
topal:
Hello,
I would need to know if when using an IOX24 module with an MC50-110n controller it is mandatory to use the SUB-CMDs of the IOX24 module for my program which is in my MC50 or else I can directly use the name of the IOX24 input?
because when I use the name of the inputs directly it does not work
and when I want to use SUB-CMd it's me who doesn't understand how to use these commands
could you help me ?
thank you
Pat
Marbek_Elektronik:
Here an example:
Marbek_Elektronik:
and this
Marbek_Elektronik:
(Perhaps you find a newer document)
The can_config of Module is important:
In example I have NodeID=0
Marbek_Elektronik:
See here
Navigation
[0] Message Index
[#] Next page
Go to full version