Author Topic: Line Spacing  (Read 3462 times)

Offline williamk

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +1/-0
Line Spacing
« on: October 21, 2021, 09:01:52 PM »
Is there any way to change the line spacing for Text Definitions that are multiple lines?

Offline williamk

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +1/-0
Re: Line Spacing
« Reply #1 on: October 21, 2021, 09:40:45 PM »
Also wondering if there's a way to vertically align text to be Center aligned instead of having it be Top aligned.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: Line Spacing
« Reply #2 on: October 22, 2021, 07:33:24 AM »
Hello williamk,

No, as far as I can see there is no setting for line spacing or vertically alignment in the definition.
We can add this to the PLUS+1 Wishlist.

Have a nice day
Best regards,
Tor
PLUS+1® SW PAE Team