Author Topic: Debug Assertion Failed  (Read 4121 times)

Offline choongKi

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +0/-0
Debug Assertion Failed
« on: March 29, 2017, 06:15:18 AM »
When I proceed Compile in PLUS+1 GUIDE, a message 'Debug Assertion Failed' appears and Compile fails.
I wonder why.

- Window version : Window 10
- Guide version : Guide 9.0.8

- Failed compile hardware : MC088-015, MC024-020, MC050-010
- Succesed compile hardware : MC050-110

Is there a solution to this problem?

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: Debug Assertion Failed
« Reply #1 on: April 04, 2017, 10:44:11 AM »
Hi ChoongKi!

I assume your Windows 10 is a Chinese version. It could deal with the different compilers used by the OS in the different hardware, MC050-110 another one. You don't happen to have a smaller project that you could try on the previously failed hardware to see if it is related to the hardware rather than the project itself?

Best regards
Nilla
PLUS+1 Helpdesk