PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 GUIDE => Topic started by: dmaris on January 25, 2013, 12:06:29 AM
-
Working on a program which I compiled without issue. Then added two I/O modules, added a bit of code, checked for errors (none found) and then tried to compile...I then get an error:
"C Compilation, Linking or LHX create of FILENAME aborted with errors"
..however there are no errors in the error tab. In fact it is completely blank.
Any suggestions?
Thanks
-
I see that once in a while. I just recompile and it goes through fine.
-
I have tried a few times but get the same result.
I did notice that although the "Error messages" tab is empty the "Build messages" tab had this in it:
Could Not Find C:\Users\DavidMaris\Plus+1 programs\build\FILENAME.out
"app2811woplink.cmd", line 150: error: run placement fails for object ".ebss",
size 0x2ffe (page 1). Available ranges:
H0SARAM size: 0x1f80 unused: 0xc2e max hole: 0xc2a
MSARAM size: 0x7c0 unused: 0x460 max hole: 0x460
LSARAM size: 0x2000 unused: 0x91b max hole: 0x91b
error: errors encountered during linking; "FILENAME.out"
not built
******************** MC24_21_MC24_24T.obj
******************** FILENAME.obj
******************** _DynamicDiagnostic.obj
******************** _NVDATA.obj
******************** _TIMEKEY.C
******************** _TIMEKEY.obj
******************** FILENAME.CMF
******************** FILENAME.out
ERROR: the last command returned code 1
WARNING: target "FILENAME.hex" not rebuild because of errors.
WARNING: target "FILENAME.hex" not rebuild because of errors.
C Compilation, Linking or LHX create of FILENAME aborted with errors
-
Found the problem...one too many IO modules...ran out of memory.
Thanks Randy